#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | tsn |
| zb_uint16_t | nwk_addr |
| zb_ieee_addr_t | ieee_addr |
| zb_uint8_t | capability |
Parameters of Device_annce primitive.
To be put into buffer as data (means - after space alloc).
| zb_uint8_t zb_zdo_device_annce_s::capability |
Capability of the local device
| zb_ieee_addr_t zb_zdo_device_annce_s::ieee_addr |
IEEE address for the Local Device
| zb_uint16_t zb_zdo_device_annce_s::nwk_addr |
NWK address for the Local Device
| zb_uint8_t zb_zdo_device_annce_s::tsn |
TSN of command