Parameters for Bind_req API call. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_ieee_addr_t | src_address |
| zb_uint8_t | src_endp |
| zb_uint16_t | cluster_id |
| zb_uint8_t | dst_addr_mode |
| zb_addr_u | dst_address |
| zb_uint8_t | dst_endp |
| zb_uint16_t | req_dst_addr |
Parameters for Bind_req API call.
| zb_uint16_t zb_zdo_bind_req_param_s::cluster_id |
The identifier of the cluster on the source device that is bound to the destination.
| zb_uint8_t zb_zdo_bind_req_param_s::dst_addr_mode |
Destination address mode bind_dst_addr_mode
| zb_addr_u zb_zdo_bind_req_param_s::dst_address |
The destination address for the binding entry.
| zb_uint8_t zb_zdo_bind_req_param_s::dst_endp |
This field shall be present only if the DstAddrMode field has a value of ZB_BIND_DST_ADDR_MODE_64_BIT_EXTENDED bind_dst_addr_mode and, if present, shall be the destination endpoint for the binding entry.
| zb_uint16_t zb_zdo_bind_req_param_s::req_dst_addr |
Destination address of the request
| zb_ieee_addr_t zb_zdo_bind_req_param_s::src_address |
The IEEE address for the source.
| zb_uint8_t zb_zdo_bind_req_param_s::src_endp |
The source endpoint for the binding entry.