Bind_req request head send to the remote. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_ieee_addr_t | src_address |
| zb_uint8_t | src_endp |
| zb_uint16_t | cluster_id |
| zb_uint8_t | dst_addr_mode |
Bind_req request head send to the remote.
| zb_uint16_t zb_zdo_bind_req_head_s::cluster_id |
The identifier of the cluster on the source device that is bound to the destination.
| zb_uint8_t zb_zdo_bind_req_head_s::dst_addr_mode |
Destination address mode bind_dst_addr_mode
| zb_ieee_addr_t zb_zdo_bind_req_head_s::src_address |
The IEEE address for the source.
| zb_uint8_t zb_zdo_bind_req_head_s::src_endp |
The source endpoint for the binding entry.