Logo
Developing with ZBOSS for Zigbee
zb_zcl_tunneling_tunnel_closure_notification_s Struct Reference

#include <zb_zcl_tunneling.h>

Data Fields

zb_uint16_t tunnel_id
 

Detailed Description

TunnelClosureNotification command payload

See also
SE spec, subclause D.6.2.5.7.2

Field Documentation

§ tunnel_id

zb_uint16_t zb_zcl_tunneling_tunnel_closure_notification_s::tunnel_id

The identifier of the tunnel that has been closed. It is the same number that has been previously returned in the response to a RequestTunnel command.


The documentation for this struct was generated from the following file: