Logo
Developing with ZBOSS for Zigbee
zb_zcl_tunneling_transfer_data_hdr_s Struct Reference

TransferData commands header data. More...

#include <zb_zcl_tunneling.h>

Data Fields

zb_uint16_t tunnel_id
 number between 0..65535 that uniquely identifies the tunnel that has been allocated in the server triggered through the RequestTunnel command. This ID must be used to send data through the tunnel or passed with any commands concerning that specific tunnel.
 

Detailed Description

TransferData commands header data.

See also
SE spec, subclause D.6.2.4.3.2
zb_zcl_tunneling_transfer_data_payload_t::hdr
TransferData client command
TransferData server command

The documentation for this struct was generated from the following file: