RequestTunnel command payload More...
#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint8_t | protocol_id |
| An enumeration representing the identifier of the metering communication protocol for which the tunnel is requested. More... | |
| zb_uint16_t | manufacturer_code |
| A code that is allocated by the Zigbee Alliance, relating the manufacturer to a device and – for the tunneling - a manufacturer specific protocol. The parameter is ignored when the ProtocolID value is less than 200. This allows for 55 manufacturer-defined protocols for each manufacturer to be defined. A value of 0xFFFF indicates that the Manufacturer Code is not used. | |
| zb_bool_t | flow_control_support |
| A boolean type parameter that indicates whether flow control support is requested from the tunnel (ZB_TRUE) or not (ZB_FALSE). The default value is FALSE (no flow control). | |
| zb_uint16_t | max_incoming_transfer_size |
| A value that defines the size, in octets, of the maximum data packet that can be transferred to the client in the payload of a single TransferData command. | |
RequestTunnel command payload
| zb_uint8_t zb_zcl_tunneling_request_tunnel_s::protocol_id |
An enumeration representing the identifier of the metering communication protocol for which the tunnel is requested.