Logo
Developing with ZBOSS for Zigbee
zb_zcl_tunneling_close_tunnel_s Struct Reference

CloseTunnel command payload More...

#include <zb_zcl_tunneling.h>

Data Fields

zb_uint16_t tunnel_id
 The identifier of the tunnel that shall be closed. It is the same number that has been previously returned in the response to a RequestTunnel command. Valid numbers range between 0..65535 and must correspond to a tunnel that is still active and maintained by the server.
 

Detailed Description

CloseTunnel command payload

See also
SE spec, subclause D.6.2.4.2.2.

The documentation for this struct was generated from the following file: