Tunneling cluster attributes. More...
#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint16_t | close_tunnel_timeout |
| CloseTunnelTimeout defines the minimum number of seconds that the server waits on an inactive tunnel before closing it on its own and freeing its resources (without waiting for the CloseTunnel command from the client). Inactive means here that the timer is re-started with each new reception of a command.0x0000 is an invalid value. More... | |
Tunneling cluster attributes.
| zb_uint16_t zb_zcl_tunneling_attrs_s::close_tunnel_timeout |
CloseTunnelTimeout defines the minimum number of seconds that the server waits on an inactive tunnel before closing it on its own and freeing its resources (without waiting for the CloseTunnel command from the client). Inactive means here that the timer is re-started with each new reception of a command.0x0000 is an invalid value.