Logo
Developing with ZBOSS for Zigbee
zb_zcl_scenes_add_scene_req_s Struct Reference

#include <zb_zcl_scenes.h>

Data Fields

zb_uint16_t group_id
 
zb_uint8_t scene_id
 
zb_uint16_t transition_time
 
zb_uint8_t scene_name [1]
 Scene name. More...
 

Detailed Description

Inform User App about Scene cluster Add Scene command.

Field Documentation

§ group_id

zb_uint16_t zb_zcl_scenes_add_scene_req_s::group_id

Scene group identifier

§ scene_id

zb_uint8_t zb_zcl_scenes_add_scene_req_s::scene_id

Scene identifier

§ scene_name

zb_uint8_t zb_zcl_scenes_add_scene_req_s::scene_name[1]

Scene name.

Has zero length (for compatibility) as unsupported attribute.

§ transition_time

zb_uint16_t zb_zcl_scenes_add_scene_req_s::transition_time

Scene transition time


The documentation for this struct was generated from the following file: