Fixed-size part of the Scene table. More...
#include <zb_zcl_scenes.h>
Data Fields | |
| zb_uint16_t | group_id |
| Group identifier for the scene. More... | |
| zb_uint16_t | transition_time |
| Scene transition time. | |
| zb_uint8_t | scene_id |
| Scene identifier. | |
| zb_uint8_t | field_sets_length |
| Field set length. More... | |
| zb_uint8_t | transition_time_100ms |
Fixed-size part of the Scene table.
| zb_uint8_t zb_zcl_scene_table_record_fixed_s::field_sets_length |
Field set length.
Actual length of the field sets. While the maximal length of the field sets is known, its actual length should be figured out in order to finish reading at a proper point. E. g.: as stated in ZCL spec, subclause 3.7.2.4.1.1, it is not mandatory for a field set to be included in the command for every cluster on the endpoint that has a defined field set. This field can provide and actual length of the field sets thus being able to read only the info required.
| zb_uint16_t zb_zcl_scene_table_record_fixed_s::group_id |
Group identifier for the scene.
Can be zero if the scene is not associated with any group