Logo
Developing with ZBOSS for Zigbee

#include <zb_zcl_commands.h>

Data Fields

zb_uint8_t direction
 
zb_uint16_t attr_id
 

Detailed Description

Format of the Attribute Status Record Field Figure 2.20 in ZCL spec. NOTE: it can be various number of attribute status record fields in Read reporting configuration request

Field Documentation

§ attr_id

zb_uint16_t zb_zcl_read_reporting_cfg_req_s::attr_id

The attribute identifier field shall contain the identifier of the attribute whose reporting configuration details are to be read.

§ direction

zb_uint8_t zb_zcl_read_reporting_cfg_req_s::direction

The direction field specifies whether values of the attribute are reported (0x00), or whether reports of the attribute are received (0x01).


The documentation for this struct was generated from the following file: