Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_publish_tier_labels_sub_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint8_t tier_id
 
zb_uint8_t tier_label [13]
 

Detailed Description

See also
SE spec, subclause D.4.2.4.9.2
zb_zcl_price_publish_tier_labels_payload_t::tier_labels

Field Documentation

§ tier_id

zb_uint8_t zb_zcl_price_publish_tier_labels_sub_payload_s::tier_id

The tier number that the associated TierLabel applies to.

§ tier_label

zb_uint8_t zb_zcl_price_publish_tier_labels_sub_payload_s::tier_label[13]

Octet String field capable of storing a 12 character string (the first character indicates the string length, represented in hexadecimal format) encoded in the UTF-8 format.


The documentation for this struct was generated from the following file: