#include <zb_zcl_price.h>
PublishTierLabels command payload
| zb_uint8_t zb_zcl_price_publish_tier_labels_payload_s::command_index |
The CommandIndex is used to count the payload fragments in the case where the entire payload does not fit into one message. The CommandIndex starts at 0 and is incremented for each fragment belonging to the same command.
| zb_uint32_t zb_zcl_price_publish_tier_labels_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint32_t zb_zcl_price_publish_tier_labels_payload_s::issuer_tariff_id |
Unique identifier generated by the commodity supplier. This is used to identify the tariff that the labels apply to.
| zb_uint8_t zb_zcl_price_publish_tier_labels_payload_s::number_of_labels |
The number of TierID/Tier Label sets contained within the command.
| zb_uint32_t zb_zcl_price_publish_tier_labels_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_zcl_price_publish_tier_labels_sub_payload_t* zb_zcl_price_publish_tier_labels_payload_s::tier_labels |
| zb_uint8_t zb_zcl_price_publish_tier_labels_payload_s::total_number_of_commands |
In the case where the entire payload does not fit into one message, the TotalNumberOfCommands field indicates the total number of sub-commands in the message.