Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_publish_price_payload_s Struct Reference

PublishPrice command payload. More...

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t provider_id
 
zb_uint8_t rate_label [13]
 
zb_uint32_t issuer_event_id
 
zb_uint32_t current_time
 
zb_uint8_t unit_of_measure
 
zb_uint16_t currency
 
zb_bitfield_t price_trailing_digit:4
 
zb_bitfield_t price_tier:4
 
zb_bitfield_t number_of_price_tiers:4
 
zb_bitfield_t register_tier:4
 
zb_uint32_t start_time
 
zb_uint16_t duration_in_minutes
 
zb_uint32_t price
 
zb_uint8_t price_ratio
 
zb_uint32_t generation_price
 
zb_uint8_t generation_price_ratio
 
zb_uint32_t alternate_cost_delivered
 
zb_uint8_t alternate_cost_unit
 
zb_uint8_t alternate_cost_trailing_digit
 
zb_uint8_t number_of_block_thresholds
 
zb_uint8_t price_control
 
zb_uint8_t number_of_generation_tiers
 
zb_uint8_t generation_tier
 
zb_uint8_t extended_number_of_price_tiers
 
zb_uint8_t extended_price_tier
 
zb_uint8_t extended_register_tier
 

Detailed Description

PublishPrice command payload.

See also
SE spec, subclause D.4.2.3.1.1.

Field Documentation

§ alternate_cost_delivered

zb_uint32_t zb_zcl_price_publish_price_payload_s::alternate_cost_delivered

Provides mechanism to describe an alternative measure of the cost of the energy consumed.

§ alternate_cost_trailing_digit

zb_uint8_t zb_zcl_price_publish_price_payload_s::alternate_cost_trailing_digit

Determines where the decimal point is located in the alternate cost field.

§ alternate_cost_unit

zb_uint8_t zb_zcl_price_publish_price_payload_s::alternate_cost_unit

Identifies the unit for Alternate Cost Delivered field (alternate_cost_delivered)

§ currency

zb_uint16_t zb_zcl_price_publish_price_payload_s::currency

Field identifying information concerning the local unit of currency used in the price field.

See also
ISO-4217

§ current_time

zb_uint32_t zb_zcl_price_publish_price_payload_s::current_time

UTC Time field containing the current time as determined by the device.

§ duration_in_minutes

zb_uint16_t zb_zcl_price_publish_price_payload_s::duration_in_minutes

Denotes amount of time in minutes after Start Time (start_time) during which the price signal is valid.

§ extended_number_of_price_tiers

zb_uint8_t zb_zcl_price_publish_price_payload_s::extended_number_of_price_tiers

Indicates a maximum number of tier available.

See also
number_of_generation_tiers

§ extended_price_tier

zb_uint8_t zb_zcl_price_publish_price_payload_s::extended_price_tier

Indicates the current price tier.

See also
price_tier

§ extended_register_tier

zb_uint8_t zb_zcl_price_publish_price_payload_s::extended_register_tier

Indicates the register tier used with the current Price Tier (register_tier).

§ generation_price

zb_uint32_t zb_zcl_price_publish_price_payload_s::generation_price

Contains the price of the commodity measured in base unit of Currency per Unit of Measure (currency per unit_of_measure) with the decimal point located as indicated by the Price Trailing Digit field (price_trailing_digit) when the commodity is received from premises.

§ generation_price_ratio

zb_uint8_t zb_zcl_price_publish_price_payload_s::generation_price_ratio

Gives the ratio of the price denoted in the Generation Price field (price) to the "normal" price, chosen by the commodity provider.

§ generation_tier

zb_uint8_t zb_zcl_price_publish_price_payload_s::generation_tier

Specifies the current generation tier.

§ issuer_event_id

zb_uint32_t zb_zcl_price_publish_price_payload_s::issuer_event_id

Unique identifier generated by the commodity provider allows devices to determine which pricing information is newer.

§ number_of_block_thresholds

zb_uint8_t zb_zcl_price_publish_price_payload_s::number_of_block_thresholds

Indicates the number of block thresholds available.

§ number_of_generation_tiers

zb_uint8_t zb_zcl_price_publish_price_payload_s::number_of_generation_tiers

Specifies the total number of generation tiers applicable in the current tariff.

§ number_of_price_tiers

zb_bitfield_t zb_zcl_price_publish_price_payload_s::number_of_price_tiers

Represents the maximum number of price tiers available.

§ price

zb_uint32_t zb_zcl_price_publish_price_payload_s::price

Contains the price of the commodity measured in base unit of Currency per Unit of Measure (currency per unit_of_measure) with the decimal point located as indicated by the Price Trailing Digit field (price_trailing_digit) when the commodity is delivered to premises.

§ price_control

zb_uint8_t zb_zcl_price_publish_price_payload_s::price_control

Identifies additional control options (PriceAcknowledgement policy and total number of tier flag).

§ price_ratio

zb_uint8_t zb_zcl_price_publish_price_payload_s::price_ratio

Gives the ratio of the price denoted in the Price field (price) to the "normal" price, chosen by the commodity provider.

§ price_tier

zb_bitfield_t zb_zcl_price_publish_price_payload_s::price_tier

Indicates the current price tier as chosen by the commodity provider

§ price_trailing_digit

zb_bitfield_t zb_zcl_price_publish_price_payload_s::price_trailing_digit

Determines where the decimal point is located in the price field

§ provider_id

zb_uint32_t zb_zcl_price_publish_price_payload_s::provider_id

Unique identifier for the commodity provider.

§ rate_label

zb_uint8_t zb_zcl_price_publish_price_payload_s::rate_label[13]

Commodity provider-specific information regarding the current billing rate.

§ register_tier

zb_bitfield_t zb_zcl_price_publish_price_payload_s::register_tier

Indicates the register tier used with the current Price Tier (price_tier).

§ start_time

zb_uint32_t zb_zcl_price_publish_price_payload_s::start_time

Denotes the time at which the signal becomes valid. Value 0x00000000 is a special time denoting "now".

§ unit_of_measure

zb_uint8_t zb_zcl_price_publish_price_payload_s::unit_of_measure

Field identifying the commodity as well as this base units of measure.

See also
enum zb_zcl_metering_unit_of_measure_e

The documentation for this struct was generated from the following file: