Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_publish_conversion_factor_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t issuer_event_id
 
zb_uint32_t start_time
 
zb_uint32_t conversion_factor
 
zb_uint8_t conversion_factor_trailing_digit
 

Detailed Description

PublishConversionFactor command payload

See also
SE spec, subclause D.4.2.4.3.1

Field Documentation

§ conversion_factor

zb_uint32_t zb_zcl_price_publish_conversion_factor_payload_s::conversion_factor
See also
SE spec, subclause D.4.2.2.4.3

§ conversion_factor_trailing_digit

zb_uint8_t zb_zcl_price_publish_conversion_factor_payload_s::conversion_factor_trailing_digit
See also
SE spec, subclause D.4.2.2.4.4

§ issuer_event_id

zb_uint32_t zb_zcl_price_publish_conversion_factor_payload_s::issuer_event_id

Unique identifier generated by the commodity provider.

§ start_time

zb_uint32_t zb_zcl_price_publish_conversion_factor_payload_s::start_time

A UTCTime field to denote the time at which the value becomes valid. The value remains valid until replaced by a newer one.


The documentation for this struct was generated from the following file: