Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_publish_co2_value_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t provider_id
 
zb_uint32_t issuer_event_id
 
zb_uint32_t start_time
 
zb_uint8_t tariff_type
 
zb_uint32_t co2_value
 
zb_uint8_t co2_value_unit
 
zb_uint8_t co2_value_trailing_digit
 

Detailed Description

PublishCO2Value command payload

See also
SE spec, subclause D.4.2.4.8.2

Field Documentation

§ co2_value

zb_uint32_t zb_zcl_price_publish_co2_value_payload_s::co2_value

The format and use of this field is the same as for the CO2 attribute or ReceivedCO2 attribute . A value of 0xFFFFFFFF indicates field not used.

§ co2_value_trailing_digit

zb_uint8_t zb_zcl_price_publish_co2_value_payload_s::co2_value_trailing_digit

The format and use of this field is the same as for the CO2TrailingDigit attribute or ReceivedCO2TrailingDigit attribute. A value of 0xFF indicates field not used.

§ co2_value_unit

zb_uint8_t zb_zcl_price_publish_co2_value_payload_s::co2_value_unit

The format and use of this field is the same as for the CO2Unit attribute or ReceivedCO2Unit attribute. A value of 0xFF indicates field not used.

§ issuer_event_id

zb_uint32_t zb_zcl_price_publish_co2_value_payload_s::issuer_event_id

Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.

§ provider_id

zb_uint32_t zb_zcl_price_publish_co2_value_payload_s::provider_id

An unsigned 32-bit field containing a unique identifier for the commodity provider.

§ start_time

zb_uint32_t zb_zcl_price_publish_co2_value_payload_s::start_time

A UTCTime field to denote the time at which the CO2 value becomes valid.

§ tariff_type

zb_uint8_t zb_zcl_price_publish_co2_value_payload_s::tariff_type

An 8-bit bitmap identifying the type of tariff published in this command. The least significant nibble represents an enumeration of the tariff type. The most significant nibble is reserved.

See also
zb_zcl_price_tariff_type_t

The documentation for this struct was generated from the following file: