Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_publish_calorific_value_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t issuer_event_id
 
zb_uint32_t start_time
 
zb_uint32_t calorific_value
 
zb_uint8_t calorific_value_unit
 
zb_uint8_t calorific_value_trailing_digit
 

Detailed Description

PublishCalorificValue command payload

See also
SE spec, subclause D.4.2.4.4.

Field Documentation

§ calorific_value

zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value
See also
sub-clause D.4.2.2.4.5

§ calorific_value_trailing_digit

zb_uint8_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value_trailing_digit
See also
sub-clause D.4.2.2.4.7

§ calorific_value_unit

zb_uint8_t zb_zcl_price_publish_calorific_value_payload_s::calorific_value_unit
See also
sub-clause D.4.2.2.4.6

§ issuer_event_id

zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::issuer_event_id

Unique identifier generated by the commodity provider.

§ start_time

zb_uint32_t zb_zcl_price_publish_calorific_value_payload_s::start_time

A UTCTime field to denote the time at which the value becomes valid. The value remains valid until replaced by a newer one.


The documentation for this struct was generated from the following file: