#include <zb_zcl_price.h>
Data Fields | |
| zb_uint32_t | latest_end_time |
| zb_uint8_t | number_of_commands |
GetCreditPayment command payload
| zb_uint32_t zb_zcl_price_get_credit_payment_payload_s::latest_end_time |
UTC timestamp indicating the latest CreditPaymentDate of records to be returned by the corresponding PublishCreditPayment commands. The first returned PublishCreditPayment command shall be the most recent record with its CreditPaymentDate equal to or older than the LatestEndTime provided.
| zb_uint8_t zb_zcl_price_get_credit_payment_payload_s::number_of_commands |
An 8-bit integer that represents the maximum number of PublishCreditPayment commands that the client is willing to receive in response to this command.