#include <zb_zcl_price.h>
Data Fields | |
| zb_uint32_t | earliest_start_time |
| zb_uint32_t | min_issuer_event_id |
| zb_uint8_t | number_of_commands |
GetConversionFactor command payload.
| zb_uint32_t zb_zcl_price_get_conversion_factor_payload_s::earliest_start_time |
UTC Timestamp indicating the earliest start time of values to be returned by the corresponding PublishConversionFactor command.
| zb_uint32_t zb_zcl_price_get_conversion_factor_payload_s::min_issuer_event_id |
A 32-bit integer representing the minimum IssuerEventID of values to be returned by the corresponding PublishCalorificValue command.
| zb_uint8_t zb_zcl_price_get_conversion_factor_payload_s::number_of_commands |
An 8-bit integer which represents the maximum number of PublishConversionFactor commands that the client is willing to receive in response to this command. A value of 0 indicates no maximum limit.