Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_get_co2_value_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t earliest_start_time
 
zb_uint32_t min_issuer_event_id
 
zb_uint8_t number_of_commands
 
zb_uint8_t tariff_type
 

Detailed Description

GetCO2Value command payload

See also
SE spec, subclause D.4.2.3.11.2

Field Documentation

§ earliest_start_time

zb_uint32_t zb_zcl_price_get_co2_value_payload_s::earliest_start_time

UTC Timestamp indicating the earliest start time of values to be returned by the corresponding PublishCO2Value command. The first returned PublishCO2Value command shall be the instance which is active or becomes active at or after the stated EarliestStartTime. If more than one instance is requested, the active and scheduled instances shall be sent with ascending ordered StartTime.

§ min_issuer_event_id

zb_uint32_t zb_zcl_price_get_co2_value_payload_s::min_issuer_event_id

A 32-bit integer representing the minimum IssuerEventID of values to be returned by the corresponding PublishCO2Value command.

§ number_of_commands

zb_uint8_t zb_zcl_price_get_co2_value_payload_s::number_of_commands

An 8-bit Integer which represents the maximum number of PublishCO2Value commands that the client is willing to receive in response to this command. A value of 0 would indicate all available PublishCO2Value commands shall be returned.

§ tariff_type

zb_uint8_t zb_zcl_price_get_co2_value_payload_s::tariff_type

An 8-bit bitmap identifying the type of tariff published in this command. The least significant nibble represents an enumeration of the tariff type.

See also
SE spec, Table D-108
zb_zcl_price_tariff_type_t

The documentation for this struct was generated from the following file: