#include <zb_zcl_price.h>
Data Fields | |
| zb_uint32_t | provider_id |
| zb_uint32_t | issuer_tariff_id |
| zb_uint8_t | tariff_type |
CancelTariff command payload
| zb_uint32_t zb_zcl_price_cancel_tariff_payload_s::issuer_tariff_id |
Unique identifier generated by the commodity Supplier. All parts of a tariff instance shall have the same IssuerTariffID.
| zb_uint32_t zb_zcl_price_cancel_tariff_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint8_t zb_zcl_price_cancel_tariff_payload_s::tariff_type |
An 8-bit bitmap identifying the type of tariff to be cancelled by this command. The least significant nibble represents an enumeration of the tariff type. The most significant nibble is reserved.