#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint32_t | provider_id |
| zb_uint32_t | issuer_event_id |
| zb_uint32_t | implementation_date |
| zb_uint32_t | max_credit_level |
| zb_uint32_t | max_credit_per_top_up |
Set Maximum Credit Limit Payload
| zb_uint32_t zb_zcl_prepayment_set_maximum_credit_limit_payload_s::implementation_date |
A UTC Time field to indicate the date from which the maximum credit level is to be applied.
| zb_uint32_t zb_zcl_prepayment_set_maximum_credit_limit_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint32_t zb_zcl_prepayment_set_maximum_credit_limit_payload_s::max_credit_level |
An unsigned 32-bit integer value indicating the maximum credit balance allowed on a meter. Any further top-up amount that will cause the meter to exceed this limit will be rejected.
| zb_uint32_t zb_zcl_prepayment_set_maximum_credit_limit_payload_s::max_credit_per_top_up |
An unsigned 32-bit integer value indicating the maximum credit per top-up. Any single top-up greater than this threshold will cause the meter to reject the top-up.
| zb_uint32_t zb_zcl_prepayment_set_maximum_credit_limit_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity supplier to whom this command relates.