Logo
Developing with ZBOSS for Zigbee
zb_zcl_prepayment_select_available_emergency_credit_payload_s Struct Reference

#include <zb_zcl_prepayment.h>

Data Fields

zb_uint32_t command_issue_date
 
zb_uint8_t originating_device
 

Detailed Description

Select Available Emergency Credit Command Payload

See also
SE spec, subclause 7.2.3.1

Field Documentation

§ command_issue_date

zb_uint32_t zb_zcl_prepayment_select_available_emergency_credit_payload_s::command_issue_date

A UTCTime field to indicate the date and time at which the selection command was issued.

§ originating_device

zb_uint8_t zb_zcl_prepayment_select_available_emergency_credit_payload_s::originating_device

An 8-bit enumeration field identifying the SE device issuing the selection command


The documentation for this struct was generated from the following file: