#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint32_t | earliest_start_time |
| zb_uint32_t | latest_end_time |
| zb_uint8_t | snapshot_offset |
| zb_uint32_t | snapshot_cause |
Get Prepay Snapshot Command Payload
| zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::earliest_start_time |
A UTC Timestamp indicating the earliest time of a snapshot to be returned by a corresponding Publish Prepay Snapshot command.
| zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::latest_end_time |
A UTC Timestamp indicating the latest time of a snapshot to be returned by a corresponding Publish Prepay Snapshot command.
| zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::snapshot_cause |
This field is used to request only snapshots for a specific cause.
| zb_uint8_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::snapshot_offset |
Where multiple snapshots satisfy the selection criteria specified by the other fields in this command, this field identifies the individual snapshot to be returned.