#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint32_t | collection_time |
| zb_uint32_t | amount_collected |
| zb_uint8_t | debt_type |
| zb_uint32_t | outstanding_debt |
Format of a Debt Payload Record
| zb_uint32_t zb_zcl_prepayment_debt_payload_record_s::amount_collected |
An unsigned 32-bit field to denote the amount of debt collected at this time.
| zb_uint32_t zb_zcl_prepayment_debt_payload_record_s::collection_time |
An UTC time field identifying the time when the collection occurred.
| zb_uint8_t zb_zcl_prepayment_debt_payload_record_s::debt_type |
An 8-bit enumeration field identifying the type of debt the record refers to. The enumerations are defined in Table D-149.
| zb_uint32_t zb_zcl_prepayment_debt_payload_record_s::outstanding_debt |
An unsigned 32-bit field to denote the amount of debt still outstanding after the debt was collected.