Logo
Developing with ZBOSS for Zigbee
zb_zcl_prepayment_credit_adjustment_payload_s Struct Reference

#include <zb_zcl_prepayment.h>

Data Fields

zb_uint32_t issuer_event_id
 
zb_uint32_t start_time
 
zb_uint8_t credit_adjustment_type
 
zb_int32_t credit_adjustment_value
 

Detailed Description

The Credit Adjustment command Payload

See also
SE spec, subclause D.7.2.3.6

Field Documentation

§ credit_adjustment_type

zb_uint8_t zb_zcl_prepayment_credit_adjustment_payload_s::credit_adjustment_type

An 8-bit enumeration field identifying the type of credit adjustment to be issued out within this command.

§ credit_adjustment_value

zb_int32_t zb_zcl_prepayment_credit_adjustment_payload_s::credit_adjustment_value

A signed 32-bit field to denote the value of the credit adjustment, measured in base unit of Currency or in Units with the decimal point

§ issuer_event_id

zb_uint32_t zb_zcl_prepayment_credit_adjustment_payload_s::issuer_event_id

Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.

§ start_time

zb_uint32_t zb_zcl_prepayment_credit_adjustment_payload_s::start_time

A UTC Time field to denote the time at which the credit adjustment settings become valid. A start date/time of 0x00000000 shall indicate that the command should be executed immediately.


The documentation for this struct was generated from the following file: