Logo
Developing with ZBOSS for Zigbee
zb_zcl_prepayment_consumer_top_up_payload_s Struct Reference

#include <zb_zcl_prepayment.h>

Data Fields

zb_uint8_t originating_device
 
zb_uint8_t top_up_code [26]
 

Detailed Description

Consumer Top Up Command is used by the IHD and the ESI as a method to apply credit top up values to a prepayment meter.

See also
SE spec, subclause D.7.2.3.5

Field Documentation

§ originating_device

zb_uint8_t zb_zcl_prepayment_consumer_top_up_payload_s::originating_device

An 8-bit enumeration field identifying the Smart Energy device issuing the selection command

See also
SE spec, Table D-146.

§ top_up_code

zb_uint8_t zb_zcl_prepayment_consumer_top_up_payload_s::top_up_code[26]

An octet string of between 1 and 26 characters (the first character indicates the string length).


The documentation for this struct was generated from the following file: