Logo
Developing with ZBOSS for Zigbee
zb_zcl_poll_control_set_short_poll_interval_req_s Struct Reference

Structure representation of Set Short Poll Interval command payload. More...

#include <zb_zcl_poll_control.h>

Data Fields

zb_uint16_t interval
 

Detailed Description

Structure representation of Set Short Poll Interval command payload.

Field Documentation

§ interval

zb_uint16_t zb_zcl_poll_control_set_short_poll_interval_req_s::interval

New Short Poll Interval


The documentation for this struct was generated from the following file: