Logo
Developing with ZBOSS for Zigbee
zb_zcl_ota_upgrade_server_remove_file_s Struct Reference

Structure representation of Data for insert OTA file to upgrade mechanism. More...

#include <zb_zcl_ota_upgrade.h>

Data Fields

zb_uint8_t endpoint
 
zb_uint8_t index
 

Detailed Description

Structure representation of Data for insert OTA file to upgrade mechanism.

Field Documentation

§ endpoint

zb_uint8_t zb_zcl_ota_upgrade_server_remove_file_s::endpoint

Endpoint

§ index

zb_uint8_t zb_zcl_ota_upgrade_server_remove_file_s::index

Index of table, index must be less value is set when create attribute


The documentation for this struct was generated from the following file: