Structure representation of Data for insert OTA file to upgrade mechanism. More...
#include <zb_zcl_ota_upgrade.h>
Data Fields | |
| zb_uint8_t | endpoint |
| zb_uint8_t | index |
| zb_uint8_t * | ota_file |
| zb_uint8_t | notify_on |
| zb_uint32_t | upgrade_time |
Structure representation of Data for insert OTA file to upgrade mechanism.
| zb_uint8_t zb_zcl_ota_upgrade_server_insert_file_s::endpoint |
Endpoint
| zb_uint8_t zb_zcl_ota_upgrade_server_insert_file_s::index |
Index of table, index must be less value is set when create attribute
| zb_uint8_t zb_zcl_ota_upgrade_server_insert_file_s::notify_on |
Flag to control Image notification after the file is inserted
| zb_uint8_t* zb_zcl_ota_upgrade_server_insert_file_s::ota_file |
OTA file, place in memory, see OTA spec 6.3.2
| zb_uint32_t zb_zcl_ota_upgrade_server_insert_file_s::upgrade_time |
Upgrade time for this OTA file