Logo
Developing with ZBOSS for Zigbee
zb_zcl_ota_upgrade_client_variable_s Struct Reference

Structure representation of client side variables. More...

#include <zb_zcl_ota_upgrade.h>

Data Fields

zb_uint32_t download_file_size
 
zb_uint16_t timer_query
 
zb_uint16_t timer_counter
 
zb_uint16_t hw_version
 
zb_uint8_t max_data_size
 
zb_uint8_t img_block_req_sent
 
zb_uint8_t pending_img_block_resp
 

Detailed Description

Structure representation of client side variables.


The documentation for this struct was generated from the following file: