Logo
Developing with ZBOSS for Zigbee
zb_zcl_on_off_off_with_effect_req_s Struct Reference

Structured representation of Off with effect command payload. More...

#include <zb_zcl_on_off.h>

Data Fields

zb_uint8_t effect_id
 
zb_uint8_t effect_variant
 

Detailed Description

Structured representation of Off with effect command payload.

Field Documentation

§ effect_id

zb_uint8_t zb_zcl_on_off_off_with_effect_req_s::effect_id

Effect identify

§ effect_variant

zb_uint8_t zb_zcl_on_off_off_with_effect_req_s::effect_variant

Effect variant


The documentation for this struct was generated from the following file: