#include <zb_zcl_metering.h>
Data Fields | |
| zb_uint8_t | interval_channel |
| zb_uint32_t | end_time |
| zb_uint8_t | number_of_periods |
GetProfile command payload
| zb_uint32_t zb_zcl_metering_get_profile_payload_s::end_time |
It is a 32-bit value (in UTCTime) used to select an Intervals block from all the Intervals blocks available.
| zb_uint8_t zb_zcl_metering_get_profile_payload_s::interval_channel |
Enumerated value used to select the quantity of interest returned by the GetProfileResponse command.
| zb_uint8_t zb_zcl_metering_get_profile_payload_s::number_of_periods |
Represents the number of intervals being requested.