#include <zb_zcl_metering.h>
Data Fields | |
| zb_uint48_t | current_summation_delivered |
| zb_uint8_t | number_of_tiers_in_use |
| zb_uint48_t * | tier_summation |
| zb_uint8_t | number_of_tiers_and_block_thresholds_in_use |
| zb_uint48_t * | tier_block_summation |
SnapshotPayloadType 6 = Block Tier Information Set Delivered (No Billing)
| zb_uint48_t zb_zcl_metering_block_tier_delivered_no_billing_payload_s::current_summation_delivered |
An unsigned 48-bit integer that returns the value of the CurrentSummationDelivered attribute at the stated snapshot timestamp.
| zb_uint8_t zb_zcl_metering_block_tier_delivered_no_billing_payload_s::number_of_tiers_and_block_thresholds_in_use |
An 8-bit BitMap representing the number of tiers and block thresholds in use at the time the snapshot was taken.
| zb_uint8_t zb_zcl_metering_block_tier_delivered_no_billing_payload_s::number_of_tiers_in_use |
An 8-bit integer representing the number of tiers in use at the time the snapshot was taken.
| zb_uint48_t* zb_zcl_metering_block_tier_delivered_no_billing_payload_s::tier_block_summation |
The Publish Snapshot command contains N elements of the Block Information Attribute Set (Delivered). The metering server shall send only the number of Tiers and Blocks in use as stated in this command.
| zb_uint48_t* zb_zcl_metering_block_tier_delivered_no_billing_payload_s::tier_summation |
The Publish Snapshot command contains N elements of CurrentTierNSummationDelivered attributes from the TOU Information Set.