§ curr_summ_delivered
| zb_uint48_t zb_zcl_metering_attrs_s::curr_summ_delivered |
§ device_type
§ status
§ summation_formatting
| zb_uint8_t zb_zcl_metering_attrs_s::summation_formatting |
SummationFormatting attribute provides a method to properly decipher the number of digits and the decimal location of the values found in the Summation Information Set of attributes.
- See also
- ZB_ZCL_ATTR_METERING_SUMMATION_FORMATTING_ID
§ unit_of_measure
| zb_uint8_t zb_zcl_metering_attrs_s::unit_of_measure |
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_stable/include/zcl/zb_zcl_metering.h