Logo
Developing with ZBOSS for Zigbee
zb_zcl_messaging_get_message_cancellation_payload_s Struct Reference

#include <zb_zcl_messaging.h>

Data Fields

zb_uint32_t earliest_implementation_time
 

Detailed Description

GetMessageCancellation command payload

See also
SE spec, subclause D.5.3.3.3.2

Field Documentation

§ earliest_implementation_time

zb_uint32_t zb_zcl_messaging_get_message_cancellation_payload_s::earliest_implementation_time

UTC Timestamp indicating the earliest implementation time of a CancelAllMessages command to be returned.


The documentation for this struct was generated from the following file: