Logo
Developing with ZBOSS for Zigbee
zb_zcl_messaging_cancel_all_message_payload_s Struct Reference

#include <zb_zcl_messaging.h>

Data Fields

zb_uint32_t implementation_date
 

Detailed Description

CancelAllMessages command payload

See also
SE spec, subclause D.5.2.3.4.2

Field Documentation

§ implementation_date

zb_uint32_t zb_zcl_messaging_cancel_all_message_payload_s::implementation_date

A UTC Time field to indicate the date/time at which all existing display messages should be cleared.


The documentation for this struct was generated from the following file: