Logo
Developing with ZBOSS for Zigbee
zb_zcl_mdu_pairing_response_s Struct Reference

Pairing Response command payload. More...

#include <zb_zcl_mdu_pairing.h>

Data Fields

zb_uint32_t lpi_version
 
zb_uint8_t total_number_of_devices
 
zb_uint8_t command_index
 
zb_uint8_t total_number_of_commands
 
zb_ieee_addr_teui64
 
zb_uint8_t num_dev_cmd
 

Detailed Description

Pairing Response command payload.

See also
SE spec, subclause 13.2.3.1

Field Documentation

§ command_index

zb_uint8_t zb_zcl_mdu_pairing_response_s::command_index

The CommandIndex is uses to count the payload fragments in the case where the entire payload does not fit into one message.

§ eui64

zb_ieee_addr_t* zb_zcl_mdu_pairing_response_s::eui64

EUI64 of Device 1 to EUI64 of Device N represent the MAC address of devices that belong to the 'virtual HAN' of the requesting device; these include the requesting device itself and all other devices the requesting device shall perform service discovery and binding with.

§ lpi_version

zb_uint32_t zb_zcl_mdu_pairing_response_s::lpi_version

Identifies the version of pairing information included in this command.

§ num_dev_cmd

zb_uint8_t zb_zcl_mdu_pairing_response_s::num_dev_cmd

Number of devices in current command

§ total_number_of_commands

zb_uint8_t zb_zcl_mdu_pairing_response_s::total_number_of_commands

In the case where the entire payload does not fit into one message, the Total Number of Commands field indicates the total number of sub-commands in the message.

§ total_number_of_devices

zb_uint8_t zb_zcl_mdu_pairing_response_s::total_number_of_devices

The total number of devices expected to form the 'virtual HAN' (including the device to which this command is being sent)


The documentation for this struct was generated from the following file: