Logo
Developing with ZBOSS for Zigbee
zb_zcl_kec_attrs_s Struct Reference

Key Establishment cluster attributes. More...

#include <zboss_api_se.h>

Data Fields

zb_uint16_t kec_suite
 Key Establishment cluster's attributes IDs. More...
 

Detailed Description

Key Establishment cluster attributes.

Field Documentation

§ kec_suite

zb_uint16_t zb_zcl_kec_attrs_s::kec_suite

Key Establishment cluster's attributes IDs.

The Information attribute set contains the attributes summarized in table below

Key Establishment Attribute Sets
Identifier Name Type Range Access Default
0x0000 KeyEstablishmentSuite 16-bit Enumeration 0x0000-0xFFFF Readonly 0x0000
See also
SE spec, C.3.1.2.2.1KeyEstablishmentSuite attribute
ZB_ZCL_ATTR_KEY_ESTABLISHMENT_SUITE_ID

The documentation for this struct was generated from the following file: