Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_zone_notification_param_s Struct Reference

Structure is used to pass parameters for ZoneStatus notification command. More...

#include <zb_zcl_ias_zone.h>

Data Fields

zb_uint8_t ep
 
zb_uint16_t status_val
 
zb_uint16_t delay
 

Detailed Description

Structure is used to pass parameters for ZoneStatus notification command.

Field Documentation

§ delay

zb_uint16_t zb_zcl_ias_zone_notification_param_s::delay

Delay

§ ep

zb_uint8_t zb_zcl_ias_zone_notification_param_s::ep

endpoint number

§ status_val

zb_uint16_t zb_zcl_ias_zone_notification_param_s::status_val

new value of zone_zone_status, see zb_zcl_ias_zone_zonestatus_e


The documentation for this struct was generated from the following file: