Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_zone_enroll_response_value_param_s Struct Reference

Declare run Enroll Response command for User Application. More...

#include <zb_zcl_ias_zone.h>

Data Fields

zb_uint8_t enroll_response
 
zb_uint8_t zone_id
 

Detailed Description

Declare run Enroll Response command for User Application.

Field Documentation

§ enroll_response

zb_uint8_t zb_zcl_ias_zone_enroll_response_value_param_s::enroll_response

Enroll response code

§ zone_id

zb_uint8_t zb_zcl_ias_zone_enroll_response_value_param_s::zone_id

Zone ID


The documentation for this struct was generated from the following file: