Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_zone_enroll_request_s Struct Reference

Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2. More...

#include <zb_zcl_ias_zone.h>

Data Fields

zb_uint16_t zone_type
 
zb_uint16_t manufacturer_code
 

Detailed Description

Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2.

Field Documentation

§ manufacturer_code

zb_uint16_t zb_zcl_ias_zone_enroll_request_s::manufacturer_code

Manufacturer code

§ zone_type

zb_uint16_t zb_zcl_ias_zone_enroll_request_s::zone_type

The documentation for this struct was generated from the following file: