Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_ace_get_panel_status_resp_s Struct Reference

Structure representsation of Get Panel Status Response command, ZCL spec 8.3.2.4.6. More...

#include <zb_zcl_ias_ace.h>

Data Fields

zb_uint8_t panel_status
 
zb_uint8_t seconds_remaining
 
zb_uint8_t aud_notification
 
zb_uint8_t alarm_status
 

Detailed Description

Structure representsation of Get Panel Status Response command, ZCL spec 8.3.2.4.6.

Field Documentation

§ alarm_status

zb_uint8_t zb_zcl_ias_ace_get_panel_status_resp_s::alarm_status

Alarm Status Field, see zb_zcl_ias_ace_alarm_status_e

§ aud_notification

zb_uint8_t zb_zcl_ias_ace_get_panel_status_resp_s::aud_notification

Audible Notification, see zb_zcl_ias_ace_aud_notification_e

§ panel_status

zb_uint8_t zb_zcl_ias_ace_get_panel_status_resp_s::panel_status

Panel Status, see zb_zcl_ias_ace_panel_status_e

§ seconds_remaining

zb_uint8_t zb_zcl_ias_ace_get_panel_status_resp_s::seconds_remaining

Seconds Remaining Parameter


The documentation for this struct was generated from the following file: