Logo
Developing with ZBOSS for Zigbee
zb_zcl_en50523_appl_ev_and_alerts_event_notif_s Struct Reference

Structure representation of Event Notification command. More...

#include <zb_zcl_en50523_appliance_events_and_alerts.h>

Data Fields

zb_uint8_t event_header
 
zb_uint8_t event_identification
 

Detailed Description

Structure representation of Event Notification command.

Parameters
event_header- Event header field
event_identification- Event Identification field, see zb_zcl_en50523_appl_ev_and_alerts_event_identification_e

The documentation for this struct was generated from the following file: