Logo
Developing with ZBOSS for Zigbee
zb_zcl_drlc_cancel_alce_payload_s Struct Reference

#include <zb_zcl_drlc.h>

Data Fields

zb_uint8_t cancel_control
 

Detailed Description

CancelAllLoadControlEvents command payload

See also
SE spec, Figure D-3

Field Documentation

§ cancel_control

zb_uint8_t zb_zcl_drlc_cancel_alce_payload_s::cancel_control

Where the Cancel Control field indicates that randomization is to be used, the receiving device should first check whether Duration Time was to be randomized and, if so, termination of the event should be adjusted according to the value of the DurationRandomizationMinutes attribute.


The documentation for this struct was generated from the following file: