Logo
Developing with ZBOSS for Zigbee

ZCL Discover Attribute Response frame. More...

#include <zb_zcl_commands.h>

Data Fields

zb_uint8_t complete
 
zb_zcl_disc_attr_info_t info [1]
 

Detailed Description

ZCL Discover Attribute Response frame.

See also
ZCL spec, zb_zcl_read_attr 2.4.15 Discover Attribute Response
Note
Command frame contains variable number of parameters

Field Documentation

§ complete

zb_uint8_t zb_zcl_disc_attr_res_s::complete

Discovery complete

§ info

zb_zcl_disc_attr_info_t zb_zcl_disc_attr_res_s::info[1]

Attribute desc list


The documentation for this struct was generated from the following file: