SetEventConfiguration Command Payload Format More...
#include <zb_zcl_device_management.h>
SetEventConfiguration Command Payload Format
| zb_uint8_t zb_zcl_device_management_set_event_cfg_cmd_payload_s::cfg_control |
The Configuration Control field allows the new configuration value to be applied to several events via a single command.
| zb_zcl_device_management_event_cfg_attr_t zb_zcl_device_management_set_event_cfg_cmd_payload_s::event_cfg |
The Event Configuration field represents the new event configuration to be applied.
| zb_zcl_device_management_set_event_cfg_payload_t* zb_zcl_device_management_set_event_cfg_cmd_payload_s::event_cfg_payload |
Set Event Configuration payload that depends on configuration control value.
| zb_uint32_t zb_zcl_device_management_set_event_cfg_cmd_payload_s::issuer_event_id |
The Issuer Event ID field represents a unique identifier generated by the commodity provider.
| zb_uint32_t zb_zcl_device_management_set_event_cfg_cmd_payload_s::start_time |
The Start Date/Time field represents a UTC date and time at which the new configuration is to be applied.