Logo
Developing with ZBOSS for Zigbee
zb_zcl_device_management_request_new_password_cmd_payload_s Struct Reference

RequestNewPassword Command Payload Format More...

#include <zb_zcl_device_management.h>

Data Fields

zb_uint8_t password_type
 

Detailed Description

RequestNewPassword Command Payload Format

See also
SE spec, subclause 10.2.3.3

Field Documentation

§ password_type

zb_uint8_t zb_zcl_device_management_request_new_password_cmd_payload_s::password_type

The Password Type field represents requested password.

See also
zb_zcl_device_management_password_type_t enum.

The documentation for this struct was generated from the following file: