Logo
Developing with ZBOSS for Zigbee

Default response payload structure. More...

#include <zb_zcl_commands.h>

Data Fields

zb_uint8_t command_id
 
zb_uint8_t status
 

Detailed Description

Default response payload structure.

Field Documentation

§ command_id

zb_uint8_t zb_zcl_default_resp_payload_s::command_id

Command identifier

§ status

zb_uint8_t zb_zcl_default_resp_payload_s::status

Command execution status


The documentation for this struct was generated from the following file: