Logo
Developing with ZBOSS for Zigbee
zb_zcl_color_control_enhanced_move_hue_req_s Struct Reference

Structure representation of Enhanced Move Hue command payload. More...

#include <zb_zcl_color_control.h>

Data Fields

zb_uint8_t move_mode
 
zb_uint16_t rate
 

Detailed Description

Structure representation of Enhanced Move Hue command payload.

See also
ZCL8 spec, subclause 5.2.2.3.16

Field Documentation

§ move_mode

zb_uint8_t zb_zcl_color_control_enhanced_move_hue_req_s::move_mode

§ rate

zb_uint16_t zb_zcl_color_control_enhanced_move_hue_req_s::rate

Rate


The documentation for this struct was generated from the following file: